Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS on February 1, 2005: RSO-M3T-NC308WA_1-050201D

A Note on Using C-Compiler Packages
M3T-NC308WA and M3T-NC30WA
--On Using the Tool for Enhancing the Scan All Dependencies Function--

Please take note of the following problem in using the M3T-NC308WA and M3T-NC30WA C-compiler packages which are used for the M16C family of MCUs:
  • On using the tool for enhancing the Scan All Dependencies function


  1. Products and Versions Concerned
    M3T-NC308WA V.5.00 Release 1 through V.5.20 Release 1
       (for the M32C/90, M32C/80, and M16C/80 series)

    M3T-NC30WA V.5.00 Release 1 through V.5.30 Release 02
       (for the M16C/60, M16C/30, M16C/20, M16C/10, M16C/Tiny,
       and R8C/Tiny series)


  2. Description
    When any of the products concerned is used in combination with the TM V.3.20 or V.3.20A, an integrated development environment, the tool for enhancing the Scan All Dependencies function may cause either of the following problem:
    (1)The enhancing tool (dependency-analyzing processor tmcpp.exe) is abnormally closed.
    (2)Header files are incorrectly displayed on the tree in the project editor.
    (3)A general protection fault, page fault, or core dump arises.


  3. Conditions
    This problem arises if either of the following conditions is satisfied:
    (1)Preprocessing directives for conditional inclusion "#if and #elif" are used, where the evaluation of the preprocessing controlling constant expression of "#if" is FALSE.
    (2)Preprocessing directives for conditional inclusion "#if and #elif" are used, where the character string including preprocessing controlling constant expression "#if" or "#elif" is equal to or greater than 512 bytes in length.

    Example:
    -----------------------------------------------------------
      #define useDef 2
    
      #if   useDef == 1
      #include "inc1.h"
      #elif useDef == 2
      #include "inc2.h"
      #endif
    
      void main(void)
      {
      }
    -----------------------------------------------------------
    In the above example, the tmcpp.exe file is abnormally closed.

  4. Workaround
    Download the problem-fixed dependency-analyzing processor (tmcpp.zip(34.3KB), an self-extracting archive).

    After decompressing it, substitute it for the existing tmcpp.exe file, which is saved in either of the following folders, where the M3T-NC308WA or M3T-NC30WA has been installed by default:
    M3T-NC308WA: \mtool\lib308
    M3T-NC30WA : \mtool\lib30 *

    * In the NC30WA V.5.30 Release 02, the tmcpp.exe file is saved in
       the \renesas\nc30wa\v530r02\lib30 folder.

    The saving directory of the tmcpp.exe file can be checked for by going through the following steps:
    (1)In the project editor, open the Project menu and select the Information command.
    (2)The Project Properties dialog box opens. Then click the Tool tab.
    (3) The value of "LIB308" or "LIB30" displayed in the Environment variables list indicates the directory where the tmcpp.exe file is saved.


  5. Schedule of Fixing the Problem
    We plan to fix this problem in our next release of the products.





© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal