Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS on February 1, 2005: RSO-E7_1-050201D

An Emulator Software Component
for the E7 Emulator
Revised to Its V.2.06 Release 00

We have revised an emulator software component for the E7 emulator from its V.2.05 Release 00 to V.2.06 Release 00.

  1. Component Concerned
    The emulator software component for the E7 emulator
       HS0007TCU01H
    which emulates the H8/300H Tiny, H8/300H SLP, H8/300L SLP, and R8C/Tiny series of MCUs.


  2. Description of Revisions
    2.1 Functions Introduced
    (1)Two channels of hardware breaking available at emulating the H8/38086RF and the H8/38076RF MCUs.
    (2)An option to execute programs without reprogramming on-chip flash memory added to the step-over function.
    (3)An option to perform the step-over function at high speed introduced. Because this option prevents reprogramming on-chip flash memory, you are able to perform the step-over function much faster.

    2.2 Problems Fixed
    Nothing


  3. How to Get and Install the Revised Component
    (1)Download the revised component from the Software Download Site.
    (2)Execute the update program to invoke the installer. Then follow its instructions.





© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal