Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS on February 16, 2005: RSO-HEW_1-050216D

A Note on Using
the High-performance Embedded Workshop

--On the Auto-backup Facilities of Workspaces--

Please take note of the following problem in using the High-performance Embedded Workshop, an integrated development environment:
  • On the auto-backup facilities of workspaces


  1. Versions Concerned
    The High-performance Embedded Workshop V.3.01.XX and 4.00.00

    To check for the version number of your High-performance Embedded Workshop, open the Help menu and select the Version of High-performance Embedded Workshop command.


  2. Description
    The auto-backup facilities of workspaces* does not operate properly. So such items of information on addition and deletion of source files and selection of tool-chain options will not be updated every specified intervals of time.
    When the High-performance Embedded Workshop is closed, in addition, the message asking whether to save the workspace does not appear, and no information on changes made to workspaces is saved on the workspace file.

    * This function, valid by default, automatically saves workspaces every specified intervals of time.

    NOTICE: When you are using the products listed below, be sure to see RENESAS TOOL NEWS "A Note on Using the High-performance Embedded Workshop--On Default Options in the Workspace Tab," issued on February 16, 2005.
    • C compiler package M3T-NC30WA V.5.30 Release 02
    • M16C R8C Debugger Package V.1.00 Release 00
    • The emulator software V.2.00 Release 00 for the E8 emulator specific to the R8C/Tiny series


  3. Workaround
    Invalidate the auto-backup facilities of workspaces at launching the High-performance Embedded Workshop. When changes are made to a workspace, save information on the changes to the workspace file by opening the File menu and selecting the Save Workspace command.


  4. Schedule of Fixing the Problem
    We plan to fix this problem in our next release of the product.





© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal