|
|
 |
RENESAS TOOL NEWS on February 16, 2005: RSO-HEW_4-050216D
A Note on Using the High-performance Embedded Workshop V.4.00.00
--On Specifying Parameters of the monitor_set Command--
|
Please take note of the following problem in using the High-performance
Embedded Workshop V.4.00.00, an integrated development environment:
- On specifying parameters of the monitor_set command
- Products Concerned
The High-performance Embedded Workshops included with the emulators
listed below and updated to V.4.00.00 using its update program are
concerned.
To check for the version number of your High-performance Embedded
Workshop, open the Help menu and select the About High-performance
Embedded Workshop command.
| (1) | The E10A-USB emulators HS0005KCU01H HS0005KCU02H Note that the problem occurs only when the emulators emulate any MCU of these groups, New_SH-Mobile, SH-4A, and SH-2A.
|
| (2) | All the E6000H emulators used in combination with the High-performance Embedded Workshop
|
| (3) | All the E6000 emulators used in combination with the High-performance Embedded Workshop Note that, in the following emulators, the problem occurs only when the optional bus monitor board is connected to each of them: HS2195EPI60H HS3008EPI60H HS3644EPI60H HS3L08EPI60H HS388REPI60H HS3800EPI60H
|
| (4) | An E200F emulator R0E0200F0EMU00 |
- Description
If the refresh_rate parameter is omitted at specifying parameters of the
monitor_set command with keywords being appended, an incorrect value of
D'01280, which indicates a refresh time interval of 1280 ms, is used as
the refresh_rate parameter, though the correct value is D'00500, which
indicates a refresh time interval of 500 ms.
Command syntax (with keywords appended):
monitor_set [name <user specific monitor-window name>] [<address>]
[<size>] [format <format>] [type <type>]
[rate <refresh_rate>] [initial_value <state>]
[detail <user specific value according to respective
Target Emulator>]
Example: monitor_set name window_a 100 10
- Workaround
Don't omit the refresh_rate parameter but enter its correct value
when you specify parameters of the monitor_set command with keywords
being appended.
Example: monitor_set name window_a 100 10 rate D'500
- Schedule of Fixing the Problem
We plan to fix this problem in our next release of the product.
|
 |