Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS on March 1, 2005: RSO-HEW_5-050301D

Supplements to Renesas Tool News
on the High-performance Embedded Workshop
Issued on January 26, 2005

--Three Problems Arising at Using the monitor_set Command Fixed--

We inform you of the supplements to RENESAS TOOL NEWS "The High-performance Embedded Workshop, an Integrated Development Environment, Revised to Its V.4.00.00," issued on January 26, 2005.
  • Three problems arising at using the monitor_set command fixed


  1. Description
    Omissions are found in Section 2.3 "Problems Fixed" in RENESAS TOOL NEWS "The High-performance Embedded Workshop, an Integrated Development Environment, Revised to Its V.4.00.00" (Doc. No. RSO-HEW-050126D), issued on January 26, 2005. Here we provide you with the supplements to the news.

    Three problems, which are described later in Section 2, arise when the monitor_set command is used in the emulators listed below. These problems has already been fixed in the High-performance Embedded Workshop V.4.00.00. So, please update yours to it using its update program.

    (1) E10A-USB emulators
      HS0005KCU01H
      HS0005KCU02H
    Note that the problems occur if any MCU of the New_SH-Mobile, SH-4A, and SH-2A groups is emulated.

    (2) E6000H emulators
    All the E6000H emulators that can be used in combination with the High-performance Embedded Workshop

    (3) E6000 emulators
    All the E6000 emulators that can be used in combination with the High-performance Embedded Workshop
    Note that in the following emulators, the problems occur only when the bus monitoring board is connected:
      HS2195EPI60H
      HS3008EPI60H
      HS3644EPI60H
      HS3L08EPI60H
      HS388REPI60H
      HS3800EPI60H

    (4) An E200F emulator
      R0E0200F0EMU00


  2. Problems Arising at Using the monitor_set Command
    The following three problems occur when the monitor_set command is used. They are fixed in the High-performance Embedded Workshop V.4.00.00, where no monitoring points are set, and an error message is displayed if the command is used.

    (1) Entering the monitor_set <monitor-window name (monitoring point name)> command displays the descriptions of a monitoring point. However, if no monitoring point is specified, a monitoring point is set all of whose parameters have their default values (for example, an address of H'0).
    Command syntax (the monitoring point name is specified):
             monitor_set [<monitor-window name>]
    Example: monitor_set monitor1
    (2) If the values of the address and size parameters exceed their maximums specified, they are set to the maximums settable in each monitoring point. Because maximum values settable are different between emulators, monitoring points having different values of parameters from your intention are set.
    Command syntax (without keywords):
             monitor_set <monitor-window name> <address> [<size>] [<format>] 
               [<refresh_rate>] [<state>] [<detail>]
    Example in CPU with 24-bit memory space: 
             monitor_set monitor1 H'FFFFFFE0 H'20
    (3) If the size parameter is not specified when the address and other parameters are specified, size is set to another value than its default of H'20 in a monitoring point.
    Command syntax (with keywords):
             monitor_set [name <monitor-window name>] [<address>] [<size>] 
                         [format <format>] [type <type>] [rate <refresh_rate>] 
                         [initial_value <state>] [detail <user specific value 
                         according to respective Target Emulator>]
    Example: monitor_set name monitor1 H'FF00 format word
    
    Workaround of Item (3):
             Specify the size parameter when specifying address and others.
    Example: monitor_set name monitor1 H'FF00 H'20 format word




© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal