Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS on March 16, 2005: RSO-M3T-NC30WA_1-050301D

The Contents of the C-Compiler Package
M3T-NC30WA V.5.30 Release 02 Modified

We have modified the contents of the C-compiler package M3T-NC30WA V.5.30 Release 02, which is used for the M16C/60, M16C/30, M16C/Tiny, M16C/20, M16C/10 and R8C/Tiny series of MCUs.

  1. Description
    1.1 AutoUpdate Utility Available
    For details, see RENESAS TOOL NEWS "The High-performance Embedded Workshop, an Integrated Development Environment, Provided with the AutoUpdate Utility," issued on March 1, 2005.

    1.2 Changes Made to the M3T-NC30WA V.5.30 Release 02
          (Revised on February 1, 2005)*
    No changes are made except the introduction of AutoUpdate utility. So, the version number remains as it is.
    * For details, see RENESAS TOOL NEWS "C Compiler Package M3T-NC30WA Revised to Its V.5.30 Release 02" issued on February 1, 2005.


  2. How to Revise Your Product
    Free-of-charge online revision is available. Please download the nc30wav530r02_2.exe file from HERE.



© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal