Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS on March 1, 2005: RSO-HEW_2-050301D

A Note on Using
the High-performance Embedded Workshop V.4.00.00

--On Docked View of the C Watch Window--

Please take note of the following problem in using the High-performance Embedded Workshop V.4.00.00, an integrated development environment:
  • On docked view of the C Watch window


  1. Product and Version Concerned
    High-performance Embedded Workshop V.4.00.00

    To check for the version number of your High-performance Embedded Workshop, open the Help menu and select the About High-performance Embedded Workshop command.


  2. Description
    If any of the following operations is performed with the C Watch window being undocked*, the High-performance Embedded Workshop abnormally shut down:
    • Switching between sessions
    • Closing a workspace
    • Terminating an application program

    * If the C Watch window is undocked, the Allow Docking check box, which appears in the pop-up menu opened by right-clicking an unoccupied portion of the window, stays unchecked. For details, see the illustration.


  3. Workaround
    Use the C Watch window in the docked state. To make the window docked, right-click an unoccupied portion of the window to open a pop-up menu, and then check the Allow Docking check box.


  4. Schedule of Fixing the Problem
    We plan to fix this problem in the next release of the product.





© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal