|
|
 |
RENESAS TOOL NEWS on March 1, 2005: RSO-HEW_3-050301D
A Note on Using the High-performance Embedded Workshop V.4.00.00
--On Saving and Restoring Symbols in the C Watch Window--
|
Please take note of the following problem in using the High-performance
Embedded Workshop V.4.00.00, an integrated development environment:
- On saving and restoring symbols entered in the C Watch window
- Product and Version Concerned
High-performance Embedded Workshop V.4.00.00
To check for the version number of your High-performance Embedded
Workshop, open the Help menu and select the About High-performance
Embedded Workshop command.
- Description
Consider that a session is saved*1 with symbols being entered in
the C Watch window. When this session is opened or refreshed*2, the
correct symbol name may not be displayed.
This problem occurs if symbol names are entered in any of the following ways:
- An element of an array is specified using square brackets ([ ]).
Example: a[0]
- A member of a structure or union is specified using a period (.).
Example: str.a
- The destination of a pointer is pointed to using a right arrow (->).
Example: pstr->a
- A pointer specifier (& or *) is used.
Example: &a or *a
For the above examples, the symbol names are all represented by "a".
NOTES:
| *1. |
Session can be saved by either of the following operations:
| (1) | Opening the File menu and then selecting the Save Session command. |
| (2) | Selecting the Session ... has been modified - do you want to save it?
dialog box, which appears by performing any of the following operations, and then clicking Yes:
(a) Switching between sessions.
(b) Closing a workspace.
(c) Terminating an application program. |
|
| *2. |
Session can be refreshed by opening the File menu and then select the Refresh Session command. |
- Workaround
If correct symbol names cannot be displayed, reenter them.
- Schedule of Fixing the Problem
We plan to fix this problem in the next release of the product.
|
 |