Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS on March 16, 2005: RSO-TOOL_2-050316D

Release of the EWS and Linux Versions
of Several Real-Time OSes, Compiler Packages,
and Assembler Packages Discontinued

We inform you that we are discontinuing the release of the EWS and Linux versions of several real-time OSes, compiler packages, and assembler packages on this April 1.

  1. Products Concerned
    1.1 For the M32R Family
    Real-time OSes M3T-MR32RK/4 and S/4*
    Compiler package M3T-CC32R

    * For the M3T-MR32RK/4 and S/4 V.4.00 Release 00, which were released on December 1, 2004, their EWS, Linux, and TurboLinux versions are not supported.

    1.2 For the M16C Family
    (1) For the M32C/90, M32C/80, and M16C/80 series
    Real-time OSes M3T-MR308K and S
    Compiler package M3T-NC308WA
    (2) For the M16C/60, M16C/30, M16C/20, M16C/10, M16C/Tiny, and R8C/Tiny series
    Real-time OSes M3T-MR30K and S
    Compiler package M3T-NC30WA

    1.3 For the 7700 Family
    (1) For the 79xx series
    Compiler package M3T-NC79WA
    (2) For the 77xx series
    Compiler package M3T-NC77WA
    Assembler package M3T-RASM77

    1.4 For the 740 Family
    Assembler package M3T-SRA74


  2. Description
    Among the products listed in Section 1 above, the release of those that run on the following host systems is discontinued:
    Host PC Host OS Comment
    IBM PC/AT or compatibleJ-Turbo linux 7 WorkstationLINUX
    HP9000 series 700HP-UX 10.x * HP700
    SPRACstationSolaris 2.5 * SOLARIS

    * Release of the related real-time OS products was discontinued in April 2004.

    For the products the release of which is discontinued, technical support will be continued except for fixing problems and improving functionality.

    We will continue usual support for the products that run on the following host systems as before:
    Host PCHost OS
    IBM PC/AT and compatibleWindows XP, Windows Me, Windows 98,
    Windows 2000, and Windows NT 4.0





© 2003-2010 Renesas Technology Corp., All rights reserved. Web Site Usage Conditions| Privacy| Sitemap