Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS on March 16, 2005: RSO-E10A-USB-050316D

The Emulator Software
for the E10A-USB Emulator
Revised to V.1.11 Release 01

We have revised the emulator software for the E10A-USB emulator to V.1.11 Release 01. (The E10A-USB emulator, whose type names are HS0005KCU01H and HS0005KCU02H, emulates the devices of the SuperH RISC engine, H8S, and H8SX families.)

  1. Emulator Concerned
    Product Type E10A-USB
    Type Names HS0005KCU01H and HS0005KCU02H
    Versions of
    Emulator Software
    V.1.08 Release 00 through V.1.11 Release 00



  2. Description of Revision
    The following problem in using the Internal Trace Function has been fixed (this problem is encountered when any CPU of the SH7206 group, SH7200 series is debugged):
    If the I-Trace button is pressed in the Trace Type area, data different from the accessed one is displayed in the Data Display area of the results of tracing.

    This problem occurs if any of the following five types of access is made:
    (1)Reading the address represented by n times 4 or n times 4 plus 1 one byte at a time using the I-Bus of the CPU.
    (2)Reading the address represented by n times 4 or n times 4 plus 2 one word at a time using the I-Bus of the CPU.
    (3)Writing the address represented by n times 4 or n times 4 plus 2 one word at a time using the I-Bus of the CPU.
    (4)Reading the address represented by n times 4 plus 2 one word at a time using the M-Bus of the CPU.
    (5)Writing the address represented by n times 4 plus 2 one word at a time using the M-Bus of the CPU.


  3. How to Revise Your Product
    Please perform the following steps:
    (1)If you have not already installed the emulator software for the E10A-USB, execute the Setup.exe file contained in your CD-ROM of the emulator software to install it.
    (2)Download the latest version of the High-performance Embedded Workshop to update yours from the Software Download Site.
    (3)Download the emulator software for the E10A-USB emulator V.1.11 Release 01 device by device* from the Software Download Site.
    (4)Execute the downloaded update program (an executable file).
    (5)For the E10A-USB, set up the emulator software (execute the Setup Tool for E10A-USB Emulator program).

    * The above-mentioned update program cannot switch the device group you are using to another one.






© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal