Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS on March 16, 2005: RSO-HEW_3-050316D

A Note on Using
the High-performance Embedded Workshop V.4.00.00

--On Using the Navigation Window--

Please take note of the following problem in using the High-performance Embedded Workshop V.4.00.00, an integrated development environment:
  • On using the Navigation window


  1. Versions Concerned
    High-performance Embedded Workshop V.4.00.00

    To check for the version number of your High-performance Embedded, Workshop open the Help menu and select the About High-performance Embedded Workshop command.


  2. Description
    If a workspace created by the High-performance Embedded Workshop V.3 or earlier is opened by its V.4.00.00 and then the category to scan (*1) is switched to another in the Select Categories dialog box (*2) of the Navigation window (*3), the High-performance Embedded Workshop terminates abnormally.

    NOTES:
    *1.The following three types exist in the categories to scan:
    C Defines
    C Functions
    C++ Classes
    *2.This dialog box appears by selecting the Select Categories command in the pop-up menu opened by right-clicking an unoccupied portion of the Navigation window.
    *3.Clicking the Navigation tab in the Workspace window opens the Navigation window.


  3. Workaround
    Switch between categories to scan with the workspace being closed*. If this operation has once been performed, you are able to switch between categories to scan while the workspace is opened.

    *: In order not to open the workspace, select Cancel in the Welcome! dialog box that appears immediately after invoking the High- performance Embedded Workshop.
    If the workspace is already opened, open the File menu and select the Close Workspace command to close it.


  4. Schedule of Fixing the Problem
    We plan to fix this problem in the next release of the product.






© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal