|
|
 |
RENESAS TOOL NEWS on March 16, 2005: RSO-SHC_2-050316D
A Note on Using the Simulator Debuggers
for the SuperH RISC Engine; and the H8, H8S, and H8SX Families
|
Please take note of a problem encountered in using the simulator debugger
for the SuperH RISC engine family and the one for the H8, H8S and H8SX
families in the same host system.
- Products and Versions Concerned
| (1) |
Simulator debugger for the SuperH RISC engine family Ver.9.0.00 and later
These simulator debuggers are included with the C/C++ compiler
package for the SuperH RISC engine family V.7.1.03 and later. |
| (2) |
Simulator debugger for the H8S and H8/300 series Ver.5.0.00 and later
These simulator debuggers are included with the C/C++ compiler
package for the H8, H8S, and H8SX families V.5.0.05 and later.
|
To check for the version number of your simulator debugger, follow
these steps:
| (1) |
In the High-performance Embedded Workshop, open the Tool menu and
select the Administration command. The Tool Administration dialog
box appears. |
| (2) |
Select the name of your simulator debugger in the Registered Components
list and click the Properties button. The Property dialog box opens. |
| (3) |
Click the Information tab, and you see the version number of yours. |
- Description
In the host system where both the simulator debuggers concerned are
installed, selecting either of them and displaying the Simulator System
dialog box may provide the message "?????????."
- 2.1 Conditions
-
| (1) |
This problem occurs in the simulator debugger for the SuperH RISC
engine family if two simulator debuggers are used in any of the
following combinations:
Version of the debugger for the SuperH RISC engine family |
Version of the debugger for the H8S and H8/300 series |
| Ver.9.0.00 or Ver.9.0.01 |
Ver.5.1.00 or later |
| Ver.9.1.01 or Ver.9.1.02 |
Ver.5.2.00 or later |
| Ver.9.2.00 |
V.5.03.00 |
| Ver.9.3.00 |
V.5.03.00 |
|
| (2) |
This problem occurs in the simulator debugger for the H8S and H8/300
series if two simulator debuggers are used in any of the following
combinations:
Version of the debugger for the H8S and H8/300 series |
Version of the debugger for the SuperH RISC engine family |
| Ver.5.0.00 |
Ver.9.1.01 or later |
| Ver.5.1.00 |
Ver.9.2.00 or later |
| Ver.5.2.00 |
Ver.9.3.01 or later |
|
- Schedule of Fixing the Problem
We plan to fix this problem in the release of the simulator debugger for
the SuperH RISC engine family V.9.05.00 and the simulator debugger for
the H8S and H8/300 series V.5.04.00.
|
 |