|
|
 |
RENESAS TOOL NEWS on April 1, 2005: RSO-E10A-USB-050401D
A Note on Using the E10A-USB and E10A Emulators
|
Please take note of the problems shown below in using the E10A-USB and E10A
Emulators, which are used for specific groups in the SuperH RISC engine family of MCUs.
- Products Concerned
| (1) |
E10A-USB and E10A emulators
for the SH7618 group, SH7600 series, SuperH RISC engine family |
| (2) |
E10A-USB emulator
for the SH7619 group, SH7600 series, SuperH RISC engine family |
Product Types:
| Product |
Product types |
| E10A-USB |
HS0005KCU01H (WithoutAUD)
HS0005KCU02H (WithAUD) |
| E10A |
HS7618KCM01H (PCMCIA)
HS7618KCI01H (PCI) |
- Problems
- 2.1 In the Case Where the E10A-USB, or the E10A of the PCMCIA Type Used
- When the HIF boot mode is used for the user system, "COMMUNICATION
TIMEOUT ERROR" arises, and the connection between the user system and
the emulator cannot be established if HIF booting is not completed
within 30 seconds after a Reset input is supplied to the user system.
So, be sure to complete HIF booting within 30 seconds upon Reset.
- 2.2 In the Case Where the E10A of the PCI Type Used
- When the HIF boot mode is used for the user system, this emulator does not function.
-
|
 |