Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS on April 1, 2005: RSO-DebuggerPackage_2-050401D

A Note on Using
the M16C R8C Debugger Package
V.1.00 Release 00

Please take note of the following problem in using the M16C R8C Debugger Package V.1.00 Release 00. This debugger package is used for the M16C/60, M16C/30, M16C/20, M16C/10, M16C/Tiny, and R8C/Tiny series of MCUs:
  • On deleting information on address-match breakpoints

  1. Description
    When the M16C R8C debugger package V.1.00 Release 00 is used in combination with a compact emulator or the PC7501 emulator, the address-match breakpoints that would have once been deleted during debugging may remain living.


  2. Solution
    This problem has already been resolved in the M16C R8C debugger package V.1.00 Release 01, so revise yours to this version.

    For details of the revision, see RENESAS TOOL NEWS "Debugger Package M16C R8C Revised to V.1.00 Release 01" No. RSO-Debugger-Package_1-050401D, issued on April 1, 2005.





© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal