Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS on April 1, 2005: RSO-DeviceUpdater-050401D

DeviceUpdater
(for High-performance Embedded Workshops Included with the SuperH RISC engine,
H8SX, H8S and H8 Family Devices)
Revised to V.1.04 Release 00

We have revised the DeviceUpdater (a tool for updating the High-performance Embedded Workshop's project files) from V.1.03 to V.1.04 Release 00.

  1. High-performance Embedded Workshops Concerned
    The High-performance Embedded Workshops included with the following products are concerned:

    (1) For the SuperH RISC engine family
    C/C++ compiler package V.7 (Windows version)
    C/C++ compiler package V.8 (Windows version)
    C/C++ compiler package V.9 (Windows version)

    (2) For the H8SX, H8S and H8 families
    C/C++ compiler package V.5 (Windows version)
    C/C++ compiler package V.6 (Windows version)



  2. Descriptions of Revision
    (1)Supported CPUs increased.
    CPUs for which the High-performance Embedded Workshop can create projects have been increased.
    (2)I/O definition files updated.
    Files that the High-performance Embedded Workshop automatically generates have been updated.
    They include I/O register definition files, header files and so on.
    For detailed information on items (1) and (2), see Update List (avairable on and after early in this April).
    (3) Introduced the function for fixing the following problem that is encountered in using a C/C++ compiler package V.6.01 Release 00 for the H8, H8S and H8SX families (avairable on and after this April 21):
    For details, see RENESAS TOOL NEWS "A Note on Using the High-performance Embedded Workshop --On Creating Assembler Project Workspaces", issued on April 1, 2005.


  3. How to Revise Your Product (Free of Charge)
    Please download the revised DeviceUpdater from HERE.
    (avairable on and after early in this April).





© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal