Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS on April 1, 2005: RSO-M3T-PD45M-050401D

Emulator Debugger M3T-PD45M
Revised to V.1.20 Release 00

We have revised the M3T-PD45M emulator debugger from V.1.10 Release 2 to V.1.20 Release 00. The M3T-PD45M is used for the 4500 series of MCUs.

  1. Descriptions of Revision
    1.1 Functions Introduced
    (1) Compact emulators are selectable for using together with the emulator debugger.
    (2) The compact emulator for the 4508 and 4509 groups--M34509T2-CPE-- has been included in the line of selectable ones.
    (3) So the following data files has been added (they are used for MCUs of the 4508 and 4509 groups):
    - M34508G4.DAT: for the 4508 group
    - M4508G4H.DAT: for the 4508 group (H version)
    - M34509G4.DAT: for the 4509 group
    - M4509G4H.DAT: for the 4509 group (H version)

    1.2 Problems Fixed
    (1) In the Register window or using the Register command, if the Z, X, or Y register is set to a value outside the range that data pointers can point to, an error arises.
    (2) If the size of the Memory window is changed while the target program is under execution, the target program may be halted.
    (3) If the target program is re-loaded, the label name appearing in the label displaying area of the Coverage window cannot be updated.

    1.3 Specification Modified
    If the value loaded in the Z, X, or Y register points to a value outside the range that data pointers can point to*, the values loaded in RAM pointed to by data pointers become not displayed in the Register window though they have hitherto been displayed.

    * The Z, X, and Y registers are used as data pointers pointing to a specific address in the RAM area in the MCU. The range that can be pointed to by data pointers varies with RAM size.

  2. How to Revise Your Product
    Free-of-charge online revision is available. So revise yours by downloading the latest version of the product from HERE and installing it.





© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal