|
|
 |
RENESAS TOOL NEWS on April 11, 2005: RSO-E8-050411D
The E8 Emulator Software
Revised to V.2.01 Release 00
|
We have revised the emulator software for the E8 on-chip debugging emulator
from V.2.00 Release 00 to V.2.01 Release 00.
- Descriptions of Revision
- 1.1 Supported MCUs Increased
- A number of MCUs in the M16C/Tiny series and M16C/60 series M16C/62P group have newly
been added to the supported line. They are as follows:
| (1) |
The M16C/Tiny series
M30260F3, M30260F6, M30260F8, M30262F3, M30262F4, M30262F6,
M30262F8, M30263F3A, M30263F6A, M30263F8A, M30280F6, M30280F8,
M30280FA, M30281F6, M30281F8, M30281FA, M30290FA, M30290FC,
M30291FA, and M30291FC
|
| (2) |
The M16C/60 series M16C/62P group
M30620FCP, M30621FCP, M30622F8P, M30623F8P, M30624FGP, M30625FGP,
M30626FHP, M30626FJP, and M30627FHP |
The E8 emulator software V.2.01 Release 00 includes the following debuggers:
- R8C/Tiny E8 Emulator debugger V.2.00.00
- M16C/Tiny, M16C/62P E8 Emulator debugger V.1.00.00
- 1.2 USB Driver Improved
- The USB driver has been improved so that the execution of the user
program can occupy the CPU of the host PC much less than before.
- 1.3 High-performance Embedded Workshop Revised
- The High-performance Embedded Workshop included with the software has
been revised from V.4.00.00 to V.4.00.01.
For details, see
RENESAS TOOL NEWS "The High-performance Embedded Workshop,
an Integrated Development Environment, Revised to V.4.00.01" No. RSO-HEW_1-050401D, issued on April 1, 2005.
- 1.4 Function Introduced
- The AutoUpdate utility supported.
For this utility, see
RENESAS TOOL NEWS "The High-performance Embedded Workshop,
an Integrated Development Environment, Provided with the AutoUpdate Utility" No. RSO-HEW_1-050301D,
issued on March 1, 2005.
- 1.5 Problem Fixed
| (1) |
When IEEE695 object files that contain relocatable object files
with no source-line information are loaded, the High-performance
Embedded Workshop is abnormally shut down.
On details of this problem, we are informing you in RENESAS TOOL
NEWS that will be issued on April 16, 2005.
|
| (2) |
The following problem has been fixed: At debugging IEEE695 object
files,no instruction except the one at the beginning address is
provided when C source statements for which the same source-line
information is generated at several addresses
(for example, a "for" statement) is displayed in MIX mode. |
- How to Revise Your Product
Free-of-charge online revision is available.
So revise yours by downloading the update program from
Software Download Site.
- Notices
| (1) |
If the update program is executed in the system where the
High-performance Embedded Workshop V.4.00.00 or earlier
resides, it will be revised to V.4.00.01.
|
| (2) |
The preview version of the M3T-NC30WA V.5.30 Release 02 C-compiler
package can be installed as a tool chain if necessary. |
|
 |