Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS on April 16, 2005: RSO-HEW_1-050416D

A Note on Using
the High-performance Embedded Workshop

--On Using the AutoUpdate Utility on Windows NT--

Please take note of the following problem in using the High-performance Embedded Workshop, an integrated development environment:
  • On using the AutoUpdate utility on Windows NT


  1. Product Concerned
    The High-performance Embedded Workshop V.4.00.00 included with the following products are concerned. They are provided with the AutoUpdate utility:

    (1) The M3T-NC308WA V.5.20 Release 02 C-compiler package
    (for the M32C/90, M32C/80, and M16C/80 series)
    (2) The M3T-NC30WA V.5.30 Release 02 C-compiler package
    (for the M16C/60, M16C/30, M16C/20, M16C/10, M16C/Tiny, and R8C/Tiny series)
    (3) The C/C++ compiler package V.9.00 Release 02 for the SuperH RISC engine family
    (4) The C/C++ compiler package V.6.01 Release 00 for the H8SX, H8S, and H8 families

    For details of the AutoUpdate utility, go to RENESAS TOOL NEWS "The High-performance Embedded Workshop, an Integrated Development Environment, Provided with the AutoUpdate Utility" issued on March 16, 2005.


  2. Description
    In the High-performance Embedded Workshop V.4.00.00 running on Windows NT, the AutoUpdate utility does not function. When invoking the utility, you will see a message saying an application error has arisen. So, click the OK button in the message box to close the utility.


  3. Solution
    This problem has already been resolved in the AutoUpdate utility included in the High-performance Embedded Workshop V.4.00.01, released on this April 1.
    The update program to the High-performance Embedded Workshop V.4.00.01 is downloadable from HERE.





© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal