Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS on May 16, 2005: RSO-DeviceUpdater-050516D

DeviceUpdater for the SuperH RISC Engine;
and H8SX, H8S, and H8 Families
Revised to V.1.05 Release 00

We have revised the DeviceUpdater from V.1.04 to V.1.05 Release 00. The DeviceUpdater is a tool for updating project files created by the High-performance Embedded Workshop.

  1. Product Concerned
    DeviceUpdater for the SuperH RISC engine; and H8SX, H8S, and H8 families, which updates project files created by the High-performance Embedded Workshops included with the following compiler packages:

    C/C++ compiler packages V.7, V.8, and V.9 for the SuperH RISC engine family (for Windows)
    C/C++ compiler packages V.5 and V.6 for the H8SX, H8S, and H8 families (for Windows)


  2. Descriptions of Revision
    (1)Supported MCUs Increased
    The following MCUs have been added to the line supported by the product:
    • SH7147F, SH7083F, SH7084F, SH7085F, and SH7086F MCUs, SH-2 core, SuperH RISC engine family
    • H8S/2189 and H8S/2239 group, H8S/2000 series, and H8S/2634 and H8S/2635 group, H8S/2600 series, H8SX, H8S, and H8 families
    You are able to browse these MCUs in the updated file list.

    (2) The capability of resolving the following problem incorporated:
    Consider the case where new projects are created using the C/C++ compiler package for the H8SX, H8S, and H8 families V.6.01 (for Windows). If compiler option -indirect is used at compiling the reset program "resetprg.c", which has been generated automatically, compile errors (Nos. C2190 and C2240) will arise.
    For details, see RENESAS TOOL NEWS "A Note on Using the C/C++ Compiler Package for the H8SX, H8S and H8 Families V.6.01 Release 00," issued on May 16, 2005.


  3. How to Revise Your Product
    Free-of-charge online revision is available. So revise yours by
    downloading the DeviceUpdater V.1.05 Release 00 from HERE.





© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal