|
|
 |
RENESAS TOOL NEWS on May 16, 2005: RSO-HEW_1-050516D
A Note on Using
the High-performance Embedded Workshop V.4
--On Viewing Command Lines at Builds-- |
Please take note of the following problem in using the High-performance
Embedded Workshop V.4, an integrated development environment:
- On viewing command lines at builds
- Product and Version Concerned
High-performance Embedded Workshop V.4
- Description
When a build is made with command lines being viewed, * no options
except assembler options are correctly displayed, and message "Can not
open sub-command file" will be displayed instead.
Though options are not displayed correctly, however, the build is
made normally.
* How to view command lines:
| (1) |
Open the Setup menu and select the Options command. |
| (2) |
The Options dialog box appears. Click the Build tab, and
check the Command line check box in the Show area. |
| (3) |
Click the OK button to close the Options dialog box. |
- Condition
This problem occurs if the High-performance Embedded Workshop V.4 is
used in combination with the M3T-NC30WA V.5.30 Release 02 C-compiler
package (which compiles the M16C/60, M16C/30, M16C/20, M16C/10,
M16C/Tiny, and R8C/Tiny series of MCUs).
- Solution
We plan to include the problem-fixed High-performance Embedded
Workshop in the next version of the M3T-NC30WA C-compiler package.
|
 |