Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS on May 16, 2005: RSO-HEW_2-050516D

A Note on Using
the High-performance Embedded Workshop V.4

--On Changing the Version of a Tool Chain to Another--

Please take note of the following problem in using the High-performance Embedded Workshop V.4, an integrated development environment:
  • On changing the version of a tool chain to another


  1. Product and Version Concerned
    The High-performance Embedded Workshop V.4


  2. Description
    For the workspaces created using the entry version of the M3T-NC308WA V.5.20 Release 1* running together with the High-performance Embedded Workshop V.4, this tool chain cannot be changed to its commercial version or to the M3T-NC308WA V.5.20 Release 2.

    * The C compiler package for the M32C/80 and M16C/80 series


  3. Workaround
    Download and decompress the problem-fixed TC.ini file (403 byte) and then overwrite the existing TC.ini file with the problem-fixed one. The existing TC.ini file is found in the System\Ts\Renesas\M32C directory under the directory where the High-performance Embedded Workshop resides.


  4. Schedule of Fixing the Problem
    We plan to fix this problem in the next release of the product.





© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal