|
|
 |
RENESAS TOOL NEWS on May 16, 2005: RSO-SHC-050516D
A Note on Using the Update Programs of
the C/C++ Compiler Packages
for the SuperH RISC Engine Family and
for the H8, H8S, and H8SX Families |
Please take note of the following problem in using the update programs of the C/C++ compiler packages (Windows versions) for the SuperH RISC engine family and for the H8, H8S, and H8SX families:
- On executing the update program
- Products Concerned
| (1) |
The shv9002u.exe update program of the C/C++ compiler package (Windows version) for the SuperH RISC engine family
(This update program is used for updating the compiler package V.9.00 Release 01 to V.9.00 Release 02) |
| (2) |
The h8v6100u.exe update program of the C/C++ compiler package (Windows version) for the H8, H8S, and H8SX families
(This update program is used for updating the compiler package V.6.00 to V.6.01 Release 00) |
- Description
Even if the shv9002u.exe or h8v6100u.exe file is executed, the new tool chain version 9.0.1.1 or 6.1.0.0 may not be installed respectively.
- Conditions
This problem occurs if either of the following conditions is satisfied:
| (1) |
The shv9002u.exe file is executed in the case where the C/C++ compiler packages for the SuperH RISC engine family V.9.00 and at least an earlier version (V.8, for instance) have been installed, and V.9.00 is not the finally installed version. |
| (2) |
The h8v6100u.exe file is executed in the case where the C/C++ compiler packages for the H8, H8S, and H8SX families V.6.00 and at least an earlier version (V.5, for instance) have been installed, and V.6.00 is not the finally installed version. |
- Workaround
This problem can be circumvented in either of the following ways:
| (1) |
If shv9002u.exe does not install the tool chain V.9.0.1.1, reinstall the C/C++ compiler package for the SuperH RISC engine family V.9.00 by overwriting the existing one.
Then execute shv9002u.exe. |
| (2) |
If h8v6100u.exe does not install the tool chain V.6.1.0.0, reinstall the C/C++ compiler package for the H8, H8S, and H8SX
families V.6.00 by overwriting the existing one. Then execute h8v6100u.exe. |
- Schedule of Fixing the Problem
We are releasing the problem-fixed update program on our tool homepage in this June.
|
 |