|
|
 |
RENESAS TOOL NEWS on June 1, 2005: RSO-SHC_2-050601D
The Update Programs of the C/C++ Compiler Packages
for the SuperH RISC engine;
and the H8, H8S, and H8SX Families Bug-Fixed |
We have fixed a bug in the update programs of the following C/C++ compiler
packages (Windows version only):
- Update program shv9002u.exe, which updates the C/C++ compiler package for
the SuperH RISC engine family to V.9.00 Release 02
- Update program h8v6100u.exe, which updates the C/C++ compiler package for
the H8, H8S, and H8SX families to V.6.01 Release 00
- Description
The problem that the execution of the above update programs does not
install new tool chains has been resolved.
For details of this problem, see RENESAS TOOL NEWS "A Note on Using the
Update Programs of the C/C++ Compiler Packages for the SuperH RISC Engine
Family and for the H8, H8S, and H8SX Families" (Doc. No. RSO-SHC-050516D),
issued on May 16, 2005.
- How to Get Bug-Fixed Programs
We are releasing the update programs on our homepage on June 6. So download
the bug-fixed shv9002u2.exe file (for the SuperH RISC engine family)
or the bug-fixed h8v6100u2.exe file (for the H8, H8S, and H8SX families)
to replace yours with it as follows:
To download shv9002u2.exe, go to
HERE.
To download h8v6100u2.exe, go to HERE.
|
 |