|
|
 |
RENESAS TOOL NEWS on June 1, 2005: RSO-M3T-ICC740-050601D
C-Compiler Package M3T-ICC740
Revised to V.1.01 Release 00 |
We have revised the M3T-ICC740 C-compiler package from V.1.00 Release 1B to V.1.01 Release 00. (The M3T-ICC740 compiles C-source programs for the 740 family of MCUs.)
- Description of Revision
The following problem has been fixed:
Problem:
A structure assignment, variable2 = variable1 via an array with pointers to struct's, went wrong.
Example:
*(structPtr->ptr) = variable;
- How to Revise Yours and Order the Revised One
- 2.1 Revision (without Charge)
- When you are using an earlier version, free-of-charge revision is available. Download the revised product from HERE.
(due to be available on and after June 20).
- 2.2 First Ordering
- When you place an order for the product, supply the following items of information to your local Renesas Technology sales office or distributor:
| Product Type: |
M3T-ICC740 |
| Version No.: |
V.1.01 |
| Release No.: |
Release 00 |
| Host OS: |
Windows XP, Windows Me, Windows 98, Windows 2000, or Windows NT 4.0 |
- On Sale of the ICC740 C-Compiler Manufactured by IAR Systems AB
IAR Systems AB has discontinued the sale of the IAR Embedded Workbench--EW740--which is used for the 740 family of MCUs. Since the EW740 includes the ICC740 C-compiler, this compiler will hereafter be soled only by Renesas Technology Corp. *
* The ICC740 C-compiler is included with Renesas's M3T-ICC740 C-compiler package.
Accordingly, be aware of the following two items concerning to the M3T-ICC740:
| (1) |
Permanent key
If you wanted to use the M3T-ICC740 after a month from the date of installation, you needed to install the permanent key issued by IAR Systems AB. Now you need not use this key.
|
| (2) |
Sales territory
Sale of the product, which was previously restricted within Japan, China, Taiwan region, and Korea, has been extended over the whole world. |
For details of the M3T-ICC740, see its datasheet.
|
 |