|
|
 |
RENESAS TOOL NEWS on July 1, 2005: RSO-E8_1-050701D
The E8 Emulator Software Revised to V.2.03 Release 00 |
We have revised the emulator software for the E8 on-chip debugging emulator
from V.2.02 Release 00 to V.2.03 Release 00.
- Descriptions of Revision
- 1.1 Supported MCUs Increased
- A number of MCUs in the H8/300H Tiny, H8/300H Super Low Power,
H8/300L Super Low Power, and R8C/Tiny series of MCUs have newly been
added to the supported line. They are as follows:
| (1) |
H8/300H Tiny series
H8/36077F |
| (2) |
H8/300H Super Low Power series
H8/38076RF, H8/38086RF, and H8/38602RF |
| (3) |
H8/300L Super Low Power series
H8/38004F, H8/38024F, H8/38104F, H8/38124F, H8/38327F,
and H8/38347F |
| (4) |
R8C/Tiny series
R5F21181, R5F21182, R5F21183, R5F21184, R5F21191, R5F21192,
R5F21193, R5F21194, R5F211A1, R5F211A2, R5F211A3, R5F211A4,
R5F211B1, R5F211B2, R5F211B3, and R5F211B4
The versions of the debuggers included with the E8 emulator
software V.2.03 Release 00 are as follows:
- R8C/Tiny E8 emulator debugger V.2.01.00
- M16C/Tiny, M16C/62P E8 emulator debugger V.1.01.00
- H8 Tiny/SLP E8 emulator debugger V.1.01.00
|
- 1.2 Functions Improved
- 1.2.1 Functions Independent of Supported MCUs
| (1) |
For the USB driver
The host PC is prevented from entering into suspended mode
during debugging. This ensures that communication between
the host PC and your emulator will not be discontinued during
debugging unless you interrupt it. |
| (2) |
For connecting two or more emulators
Two or more E8 emulators can be connected to the host PC.
This enables you to debug several programs in parallel. |
1.2.2 Functions in the R8C/Tiny E8 Emulator Debugger
| (1) |
Format of displaying IO definition files modified
IO definition files are displayed in bit-field format in
the IO window. |
| (2) |
The Cancel button added
The Cancel button has been added to the Select Emulator
mode dialog box, which appears when you open the Debug menu and
select the Connect command. |
1.2.3 Functions in the M16C/Tiny, M16C/62P E8 Emulator Debugger
| (1) |
Working RAM area reduced in size
The working RAM area used by the firmware in the target MCU has
been reduced from 256 bytes to 128 bytes. As a result, the number
of digits for setting the working RAM area has been modified in
the Firmware Location & WDT dialog box,* which is displayed
during combining the emulator debugger with the firmware in
the E8 emulator.
* Automatically displayed during combining the emulator debugger
with the firmware in the E8. |
| (2) |
Speedup of run-time debug processing
The speed of run-time debug processing (memory dumps and memory
fills) during executing user programs has been boosted. |
1.2.4 Function in the H8 Tiny/SLP E8 Emulator Debugger
| (1) |
Verification of memory fills
Memory fills can be verified when a verify option is selected
at executing memory fills. |
- 1.3 Problem Fixed
- The following problem, which is independent of supported MCUs, has
been fixed:
When IEEE695 objects are loaded, information about
structures exceeding 128 bytes in size cannot properly be provided
in the Watch and Local windows.
For details see RENESAS TOOL NEWS Doc. No. RSO-E8_2-050701D,
issued on July 1, 2005. (available on and after this July 22)
- How to Update Yours
When you are using a previous version, free-of-charge online revision
is available.
Download the update program from
HERE and update yours.
- Notices
| (1) |
If the update program is executed in the system where the
High-performance Embedded Workshop V.4.00.00 or earlier
resides, it will be revised to V.4.00.01. |
| (2) |
The update program can install the evaluation version of the
M3T-NC30WA V.5.30 Release 02 C-compiler package as a tool chain
if you need it. |
|
 |