|
|
 |
RENESAS TOOL NEWS on July 16, 2005: RSO-TOOL_1-050716D
A Correction to E8 Emulator Additional
Document for User's Manual
Notes on Connecting the H8/38076RF
and H8/38086RF |
We notify a correction to E8 Emulator Additional Document for User's Manual, Notes on Connecting the H8/38076RF and H8/38086RF (Document No. REJ10B0213-0100).
- Page 7, the first line
Read
| |
The emulator need to use the RES# pin. So build the circuit shown in Figure 3.4 in order that the emulator can accept reset inputs. |
for
| |
The RES# pin is used by the emulator. Create the following circuit by connecting the open-collector output buffer so that reset input can be accepted from the emulator. |
- Schedule of Revising the Manual
We plan to revise this misdescription in the next revision of the manual.
|
 |