|
|
 |
RENESAS TOOL NEWS on July 16, 2005: RSO-Debugging Extension-050716D
The Real-Time OS Debugger
"Debugging Extension"
Revised to V.1.05 Release 00 |
We have revised the Debugging Extension from V.1.04 Release 00 to V.1.05 Release 00.
The Debugging Extension is a software tool for adding capabilities of debugging real-time OSes to the High-performance Embedded Workshop.
- Description of Revision
Real-time OS "T-Kernel" supported.
The T-Kernel is used for the SuperH family of T-Engine devices. So these devices can be targeted for debugging.
- Supported Real-Time OSes and Versions of the High-performance Embedded Workshop
-
-
- 2.1 Real-Time OSes
-
- HI7000/4, HI7700/4, HI7750/4 and T-Kernel (for the SuperH family)
- HI1000/4 (for the H8SX family)
- HI2000/3 (for the H8S family)
- 2.2 High-performance Embedded Workshop
V.3 or later
- If you are using the product earlier than V.3, update it to V.3 or later. Free-of-charge online update is available from Software Download Site.
- How to Update Your "Debugging Extension"
Free-of-charge online update is available. So download the revised program to update yours from HERE.
- How to Introduce "Debugging Extension" From Scratch
Download the latest program from the Web site shown in Section 3 above.
|
 |