|
|
 |
RENESAS TOOL NEWS on July 16, 2005: RSO-E8_1-050716D
The E8 Emulator Software
Revised to V.2.03 Release 01 |
We have revised the emulator software for the E8 on-chip debugging emulator from V.2.03 Release 00 to V.2.03 Release 01.
- Description of Revision
The problem on debugging the R8C/14 and R8C/16 groups of MCUs has been fixed.
For details, see RENESAS TOOL NEWS "A Note on Using the E8 Emulator Software V.2.03 Release 00" No. RSO-E8_2-050716D, issued on July 16, 2005.
- How to Update Your Product
Free-of-charge online update is available. So download the update program to update yours from "E8 Emulator Debugger Online Upgrade".
- Notices
| (1) |
If the update program is executed in the system where the High-performance Embedded Workshop V.4.00.00 or earlier resides, it will be updated to V.4.00.01. |
| (2) |
The revised program can install the evaluation version of the M3T-NC30WA V.5.30 Release 02 C-compiler package as a tool chain if you want it. |
|
 |