Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS on August 1, 2005: RSO-E8-050801D

The E8 Emulator Software
Revised to V.2.04 Release 00

We have revised the emulator software for the E8 on-chip debugging emulator from V.2.03 Release 01 to V.2.04 Release 00.

  1. Descriptions of Revision
    1.1 Supported MCUs Increased
    A number of MCUs in the M32C/80 series have newly been added to the supported line. They are as follows:
    (1) M32C/84 group
    M30843FW, M30843FH, M30843FJ, M30845FW, M30845FH, and M30845FJ
    (2) M32C/85 group
    M30853FW, M30853FH, M30853FJ, M30855FW, M30855FH, and M30855FJ
    (3) M32C/86 group
    M30865FJ
    (4) M32C/87 group
    M30879FL and M3087BFL
    (5) M32C/88 group
    M30880FW, M30882FW, M30880FH, M30882FH, M30880FJ, and M30882FJ

    1.2 Debuggers Included with the Product Updated
    The M32C/80 E8 emulator debugger has newly been included with the emulator software. So the debuggers included with it and their versions are as follows:
    • R8C/Tiny E8 emulator debugger V.2.01.01
    • M16C/Tiny, M16C/62P E8 emulator debugger V.1.01.00
    • H8 Tiny/Super Low Power E8 emulator debugger V.1.01.00
    • M32C/80 E8 emulator debugger V.1.00.00

    1.3 The High-performance Embedded Workshop Revised
    The High-performance Embedded Workshop bundled with the software has been revised from V.4.00.01 to V.4.00.02.
    For details, see RENESAS TOOL NEWS "The High-performance Embedded Workshop, an Integrated Development Environment, Revised to V.4.00.02" NO. RSO-HEW-050701D, issued on July 1, 2005.


  2. How to Update Your Product
    Free-of-charge online update is available. So download the revised program to update yours from "E8 Emulator Debugger Online Upgrade".


  3. Notices
    (1) If the revised program is installed in the system where the High-performance Embedded Workshop V.4.00.01 or earlier resides, it will be updated to V.4.00.02.
    (2) The revised program can install the evaluation version of the M3T-NC30WA V.5.30 Release 02 C-compiler package as a tool chain if desired.





© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal