Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS on August 16, 2005: RSO-M30870T2-CPE-050816D

Information on Our Compact Emulators
Bearing the CE Marking

We inform you of the product types of our compact emulators that have been allowed to bear the CE marking.*

*   The products conforming to the EC directives are allowed to bear the CE marking. In order to export products to European countries, it is necessary that they be bearing the CE marking.


  1. Products Concerned
    The following compact emulators have been allowed to bear the CE marking:
    (1)   R0E436640CPE00 (for the H8/300H Tiny series)
    (2)   M30850T2-CPE (for the M32C/84, M32C/85, and M32C/86 groups)
    (3)   M30870T2-CPE (for the M32C/87 group)
    (4)   M30290T2-CPE (for the M16C/Tiny series)
    (5)   M38000T2-CPE (for the 740 family)


  2. Shipment of the Products Concerned
    We started the shipment of the products listed in (1), (2), and (3) above that bear the CE marking on August 22. And we have already been shipping the products listed in (4) and (5) above that conform to the CE Marking.


  3. Standards
    The products concerned meet the following two standards:
    (1)   EN55022: 1998 Class A
    (2)   EN55024: 1998


    Notices on using any product bearing the CE marking:
    • Electrostatic Discharge Precautions must be taken when handling the product.
    • Must not be used within 30 meters of a domestic radio or television receiver.
    • For correct operation of this product, it is recommended that Mobile phones are not used within 10 meters of the product system.
    • This product should be powered down when not in use.


  4. Other
    No changes have been made to the products concerned except that they bear the CE marking. The ordering information about them and their prices remain as before.





© 2003-2010 Renesas Technology Corp., All rights reserved. Web Site Usage Conditions| Privacy| Sitemap