|
|
 |
RENESAS TOOL NEWS on September 1, 2005: RSO-H8C-050901D
The C/C++ Compiler Packages for the H8, H8S,
and H8SX MCU Families Revised to V.6.01 Release 01 |
The C/C++ compiler packages for the H8, H8S, and H8SX MCU families have been revised from V.6.01 Release 00 to V.6.01 Release 01.
- Products Concerned
The H8, H8S, and H8SX MCU families C/C++ compiler packages V.6. (Products for Windows, Solaris, and HP-UX concerned.)
- Descriptions of Revision
| 2.1 |
|
Functions Introduced and Improved
|
| 2.2 |
|
Problems Fixed
The problems described in Sections 2.2.1 through 2.2.4 below have been fixed.
| 2.2.1 |
|
In the Installer (Windows Version Only)
On executing the batch file for setting environmental variables
For details, see RENESAS TOOL NEWS "A Note on Using the C/C++ Compiler Packages
for the SuperH RISC Engine; and the H8, H8S and H8SX Families (Windows Versions Only)" (No. RSO-SHC_1-050316D), issued on March 16, 2005.
|
| 2.2.2 |
|
In the Simulator (Windows Version Only)
| (1) |
|
On using the simulator debugger for the SuperH RISC engine family and the one for the H8, H8S and H8SX families in the same host system For details, see RENESAS TOOL NEWS "A Note on Using the Simulator Debuggers for the SuperH RISC Engine; and the H8, H8S, and H8SX Families" (No. RSO-SHC_2-050316D), issued on March 16, 2005. |
| (2) |
|
On setting access to memory resources For details, see RENESAS TOOL NEWS "A Note on Using the Simulator Debugger for the SuperH RISC Engine; and for the H8S Families and the H8/300 Series of MCUs--On Setting Access to Memory Resources" (No. RSO-SH-SIM-050416D), issued on April 16, 2005. |
| (3) |
|
On accessing system control register SYSCR For details, see RENESAS TOOL NEWS "A Note on Using the Simulator Debugger for the H8S Family and H8/300 Series of MCUs--On Accessing System Control Register SYSCR" (No. RSO-H8SX-SIM- 050416D), issued on April 16, 2005. |
| (4) |
|
On searching for trace records For details, see RENESAS TOOL NEWS "A Note on Using the Simulator Debugger for the H8S Family and H8/300 Series of MCUs--On Searching for Trace Records" (No. RSO-H8S-SIM-050416D), issued on April 16, 2005, |
|
| 2.2.3 |
|
In the Compilers
| (1) |
|
Eight problems reported in RENESAS TOOL NEWS "Notes on Using the C/C++ Compiler Package V.6 for the H8SX, H8S, and H8 Families of MCUs" (No. RSO-H8C-050716D), issued on July 16, 2005. |
| (2) |
|
On referencing incorrect memory area For details, see RENESAS TOOL NEWS "A Note on Using the C/C++ Compiler Package V.6 for the H8SX, H8S, and H8 Families" (No. RSO-H8C-050801D), issued on August 1, 2005. |
| (3) |
|
Also the following four problems resolved:
- On incorrectly displaying information on the register that contains the values of variables and union-type ones on the debugger because the compiler generates incorrect debug information
- On displaying errors C2190, C2240, C4712, and C2238 accidentally
- On not displaying error C2311 when it arises
- On displaying assemble errors (W)835 or (E)526 when assembly programs generated by the compiler are assembled
|
|
| 2.2.4 |
|
In the Linker (Optimizing Linkage Editor optlnk)
| (1) |
|
On linkage list files generated by the optimizing linkage editor
For details, see RENESAS TOOL NEWS "A Note on Using the Optimizing Linkage Editor for the SuperH RISC Engine,
H8, H8S, and H8SX Families of MCUs" (No. RSO-SHC-050416D), issued on April 16, 2005.
|
| (2) |
|
On displaying the error message shown below accidentally ** L0103 (I) Multiple stack sizes specified to the symbol "Function Name"
Conditions:
This problem may occur if the following conditions are all satisfied:
- The version of the linker is V.9.00.00 or later.*
- An extern-qualified variable that has the same name as a function defined in a C/C++ source file exists in another C/C++ source file. Or, an import label of "_<Function Name>" exists in an assembly source file.
- The message option is used at linking.
- Also the stack option is used at linking.
|
| (3) |
|
On generating an incorrect stack information file (.sni) Conditions:
This problem may occur if the following conditions are all satisfied:
- The version of the linker is V.9.00.00 or later.*
- An extern-qualified variable that has the same name as a function defined in a C/C++ source file exists in another C/C++ source file. Or, an import label of "_<Function Name>" exists in an assembly source file.
- The stack option is used at linking.
NOTICE:
If an incorrect .sni file is read into the stack analyzing tool, Call Walker, incorrect stack usage is provided.
|
| (4) |
|
On generating incorrect object code by using the "optimize=symbol _delete" option to optimize the deletion of unreferenced symbols
Conditions:
This problem may occur if the following conditions are all satisfied:
- The version of the linker is V.9.00.00 or later.*
- The optimize option is used at compilation.
- Also the pack=1 option is used at compilation, or "#pragma pack 1" is put in a C/C++ source file.
- Optimization of the deletion of unreferenced symbols is valid in the linker.
Optimization becomes valid in any of the following cases:
- The optimize=symbol_delete option is used.
- The optimize=speed option is used.
- The optimize option is used.
- The nooptimize option is not used.
- Constants (const- qualified variables) and variables having their initial values are deleted as unreferenced variables by the optimization in Condition 4.
|
| (5) |
|
On generating incorrect debug information by using the compress option to compress debug information
Conditions:
This problem may occur if the following conditions are all satisfied:
- The version of the linker is V.9.00.00 or later.*
- The "debug" option is used at compilation.
- Also the "compress" option is used for generating relocatable files (.rel) at linking.
- The relocatable files in Condition 3 are read into the linker to generate a load module using the "compress" option.
NOTICE:
Loading the above load module in the debugger results in errors.
|
| (6) |
|
Also the problem that internal errors arise if any of the following conditions is met is resolved:
- The linker reads .rel files written in the assembly language and containing .EQU symbols (internal error L4000-8010).
- The linker reads object files containing function calls calling .EQU symbols (internal error L4000-8874).
- The linker reads .rel files (internal error L4000-8027 or L4001).
|
|
* How to check for the version number of your linker
| (1) |
|
In the High-performance Embedded Workshop, open the Tool menu and select the Administration command. The Tool Administration dialog box appears. |
| (2) |
|
Out of the Toolchains tree in the Registered Components list, select the name of the compiler package you are using; then click the properties button. |
| (3) |
|
Click the Information tab in the Properties dialog box, and you see the version number of your linker.
Example of Display: Optimizing Linkage Editor (V.9.00.02) |
|
- How to Update Your Package and Purchase the Revised One
| 3.1 |
Free-of-Charge Update
Free-of-charge update is available if you are using the product concerned.
| (1) |
|
Windows version To update yours online, download the revised product from HERE. |
| (2) |
|
Solaris and HP-UX versions Supply the following items of information to your local Renesas Technology sales office or distributor. We will send you the latest version of the product package by return:
| Type Name |
Solaris or HP-UX version |
| Version No. |
V.6.01 |
| Release No. |
Release 01 |
|
|
| 3.2 |
First Ordering
If you place an order for any of the products, please supply the following items of information to your local Renesas Technology sales office or distributor:
| Type Name |
Windows, Solaris, or HP-UX version |
| Version No. |
V.6.01 |
| Release No. |
Release 01 |
|
|
 |