Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS on September 1, 2005: RSO-HEW_2-050901D

A Note on Using
the High-performance Embedded Workshop
--On the Tooltip Watch Function-

Please take note of the following problem in using the High-performance Embedded Workshop, an integrated development environment:
  • On the Tooltip Watch function*
*   This function is used for referencing values of the variables defined in the source program. To do so, display the source program that contains the variable whose value you want to reference in the Editor window; then hover your mouse pointer over the variable's name. The value of the variable will be told in the pop-up window as a tip.

  1. Version Concerned
    High-performance Embedded Workshop* V.4.00.02

    *   The High-performance Embedded Workshop is bundled with the software products (a C compiler and others) that support it.

    To check for the version number of your High-performance Embedded Workshop, open the Help menu and select the About High-performance Embedded Workshop command.


  2. Description
    Suppose that the value of a variable were separated into 1-byte blocks, and the value of any block fell within a range of 0x80--0xff. If this variable is displayed in the Editor window using the Tooltip Watch function, the values of all the upper 1-byte blocks to the left of the above-mentioned block will be represented by 0xff in a 64-bit value.

    Examples of representation in hexadecimal notation:
    Value of Variable Value Represented
    Using Tooltip Watch Function
    0x7f7f7f80 0xffffffffffffff80
    0x807f 0xffffffffffff807f
    0x80 0xffffffffffffff80


  3. Conditions
    This problem occurs if the product concerned is used in combination with the following products:

    (1)   C/C++ compiler pckage for the SuperH RISC engine family V.7.1.01 through V.9.00 Release 03
    (2)   C/C++ compiler package for the H8, H8S, and H8SX families V.5.0.03 through V.6.01 Release 01
    (3)   E10A-USB emulators
    HS0005KCU01H
    HS0005KCU02H
    NOTICE:
    Be sure to see Section 4, "To the Users Who Are Using the E10A-USB Emulator," in RENESAS TOOL NEWS "The High-performance Embedded Workshop, an Integrated Development Environment, Revised to Its V.4.00.00" (No. RSO-HEW-050126D), issued on January 26, 2005.
    (4)   E7 emulator
    HS0007TCU01H
    (5)   E8 emulator
    R0E000080KCE00
    (6)   E6000H emulators
    All the versions for the High-performance Embedded Workshop
    (7)   E6000 emulators
    All the versions for the High-performance Embedded Workshop
    (8)   E10A emulators
    All the versions for the High-performance Embedded Workshop
    (9)   E10T emulators
    All the versions for the High-performance Embedded Workshop
    (10)   E10T-USB emulator
    HS0005TCU01H
    (11)   E200F emulators
    R0E0200F0EMU00
    R0E0200F1EMU00


  4. Workaround
    Use the Instant Watch function* instead of the Tooltip Watch function. The Instant Watch function can also reference values of the variables defined in the source program.

    * To use this function, follow these steps:
    (1)   Select the variable whose value you want to reference in the Editor window.
    (2)   Right-click an unoccupied area of the Editor window to open a pop-up menu.
    (3)   In the menu, select the Instant Watch command. The Instant Watch dialog box will appear.


  5. Schedule of Fixing the Problem
    We plan to fix this problem in the next release of the product.





© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal