Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS on September 1, 2005: RSO-SHC-050901D

A Note on Using
the SuperH RISC Engine Family
C/C++ Compiler Package V.9

Please take note of the following problem in using the C/C++ compiler package for the SuperH RISC engine family of MCUs:
  • On displaying an HTML file after installing the product package


  1. Product and Versions Concerned
    Windows edition of the SuperH RISC engine family C/C++ compiler package V.9.00 Release 02 and later


  2. Description
    Immediately after the compiler package has been installed, normally the HTML file with a title of "About change of the toolchain name" is displayed by the browser. However, if your host OS is Windows NT, the browser cannot be invoked, resulting in the HTML file being not provided.


  3. Workaround
    Normally the HTML file displayed after installing the compiler package is located at

      InstallDirectory\Support\InstallGuide_E.html

    So open this file by the browser.





© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal