Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS on September 1, 2005: RSO-E7_2-050901D

A Note on Using
the E7 Emulator Software V.3.00 Release 00

Please take note of the following problem in using the emulator software for the E7 on-chip debugging emulator (the E7 emulator is used for the H8/300H Tiny, H8/300H Super Low Power, and H8/300L Super Low Power Series of MCUs):
  • On Debugging Programs for the H8/300H Tiny, H8/300H Super Low Power, and H8/300L Super Low Power Series of MCUs


  1. Product and Version Concerned
    The E7 emulator software V.3.00 Release 00


  2. Problem
    The MCU names of the support MCU series (H8/300H Tiny, H8/300H Super Low Power, and H8/300L Super Low Power Series) added to those in V.2.0.01 cannot be displayed in the Device dropdown list in the Select Emulator Mode dialog box.*

    *   To open this dialog box, click the Debug menu name and select the Connect command in the High-performance Embdded Workshop.


  3. Condition
    This problem occurs if the emulator software V.3.00 Release 00 is installed in the PC where V.2.0.00 or earlier resides.


  4. Solution
    This problem has already been resolved in the emulator software V.3.00 Release 01. So download the update program from Software Download Site and install it.





© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal