Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS on September 16, 2005: RSO-Debugging Extension-050916D

The Real-time OS Debugger
Debugging Extension
Revised to V.1.06 Release 00

The real-time OS debugger Debugging Extension has been revised from V.1.05 Release 00 to V.1.06 Release 00.
The Debugging Extension is the software product for adding the debugging functions of real-time OSes to the High-performance Embedded Workshop. For details of the specifications of the product, see its datasheet.

  1. Descriptions of Revision
    • The real-time OS HI7000/4 V.2.01 Release 00 has been supported. (This real-time OS is used for the SuperH family of MCUs.)
    • The representation of the interrupt definition numbers, which are displayed in the Interrupt Handler window, has been changed from hexadecimal notation to decimal one (only when HI7000/4 targeted).


  2. Supported Real-time OSes and High-performance Embedded Workshop
    The following have been supported.

    2.1   Real-time OSes
    • HI7000/4, HI7700/4, HI7750/4 and T-Kernel (for the SuperH family)
    • HI1000/4 (for the H8SX family)
    • HI2000/3 (for the H8S family)
    2.2   High-performance Embedded Workshop
    V.3 and later
    If you are using any version earlier than V.3, upgrade it to V.3 or later free of charge by visiting HERE.


  3. How to Update Your Product
    Free-of-charge online update is available. So download the revised program to update yours from HERE.


  4. First-time installation of the Product
    Download and install the Debugging Extension the same way shown in 3 above.





© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal