Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS on September 16, 2005: RSO-M38000T2-CPE-050916D

New MCUs Supported
by the Compact Emulator M38000T2-CPE

A number of MCUs in the 740 family have newly been added to the line supported by the M38000T2-CPE compact emulator.

  1. Description
    MCU Group Emulator MCU *1 MCU File
    3826 M38267RLFS M38000.MCU *2
    3885 M38859RLFS M38000.MCU *2
    3886 M38867RFS M38000.MCU *2
    38K2 M38K29RFS M38000.MCU *2
    38C8 M38C89RLFS M38000.MCU *2
    7516 M37516RSS M37516.MCU *3
    7517 M37517RLSS M37517.MCU *3
    7560 M37560RLFS M37560.MCU *3
    M37151 M37151ERSS M37151.MCU *3
    M37161 M37161ERSS M37161.MCU *3
    M37221 M37221EARSS M37221.MCU *3
    M37225 M37225ERSS M37225.MCU *3
    M37280 M37280ERSS M37280.MCU *3

    NOTES:
    *1.   These emulator MCUs are optional.
    *2.   These MCU files are provided by the M3T-PD38M emulator debugger, which is included with the M38000T2-CPE.
    *3.   Download mcu_files.zip (2.41 KB).

    For the guaranteed operational conditions of the M38000T2-CPE with any of the emulator MCUs listed above, visit M38000T2-CPE User's Manual(Compact Emulator for 740 Family). See "4.2 Applicable MCU" (P.50 -- P.64).


  2. Update of the Firmware
    If you are using the M38000A1.C0 firmware whose version is earlier than 1.03.00, update it to the latest version.
    To check for the version number of your M38000A1.C0 firmware, launch the M3T-PD38M emulator debugger; then select [Help] -> [About] menu. The latest M3T-PD38M comes with the M38000A1.C0 firmware of Ver.1.02.00.

    The procedure for updating the firmware is as follows:

    (1)   Download the firmware file firm.exe (163 KB).
    (2)   Decompress the firm.exe file; then follow the instructions described in the Readme_e.txt file.


  3. Related News





© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal