|
|
 |
RENESAS TOOL NEWS on October 1, 2005: RSO-DebuggerPackage-051001D
The Emulator Debuggers
for the M16C/60, /30, /Tiny, /20, /10,
and R8C/Tiny Series
Revised to V.1.01 Release 00 |
The emulator debuggers for the M16C/60, /30, /Tiny, /20, /10, and R8C/Tiny series have been revised to those listed below.
- M16C R8C PC7501 emulator debugger V.1.01 Release 00
- M16C PC4701 emulator debugger V.1.01 Release 00
- M16C R8C compact emulator debugger V.1.01 Release 00
- M16C R8C FoUSB/UART debugger V.1.01 Release 00
- Descriptions of Revision
| 1.1 |
|
Functions Introduced and Improved
For the functions improved, see the version report described in the release note of each debugger. |
| |
|
|
| 1.2 |
|
Problems Fixed
Many problems have been fixed by the revision of the High-performance Embedded Workshop. For these see the following items of news:
NOTICE:
The problem "On debugging a target system serially connected to the host PC," which was notified in the news with Document No. RSO- DebuggerPackage-050416D, issued on this April 16, remains as before; that is, up to two breakpoints can be set in the R8C/14, R8C/15, R8C/16, and R8C/17 groups of MCUs. However, up to four breakpoints are usable in the R8C/18, /19, /1A, and /1B groups. |
- How to Update Yours
Free-of-charge online update is available. So download the revised program you want to update yours from its software download site shown below.
|
 |