|
|
 |
RENESAS TOOL NEWS on October 16, 2005: RSO-E10A-USB-051016D
The E10A-USB Emulator Software
Revised to V.2.01 Release 00 |
We have revised the emulator software for the E10A-USB emulators
(HS0005KCU01H and HS0005KCU02H) to V.2.01 Release 00. These emulators are
used for the SuperH RISC engine, H8S, and H8SX families of MCUs.
- Versions Concerned
Emulator software V1.0.00 through V.2.00 Release 03
for the E10A-USB emulators (HS0005KCU01H and HS0005KCU02H)
- Descriptions of Revision
The following devices have been added to the support line of five
device groups:
| Device Group | MCUs |
| H8S | H8S/2189RF |
| H8SX | H8SX/1653F |
| SH-2 | SH7606 |
| SH-4A | SH7763 |
| New_SH-Mobile | SH7343, SH7348 |
- How to Update Your Product
| (1) |
|
If you have not already installed the emulator software for the
E10A-USB, execute the Setup.exe file contained in your CD-ROM of
the emulator software to install it. |
| (2) |
|
Download the update program to the E10A-USB emulator software
V.2.01 Release 00 device by device from HERE. |
| (3) |
|
Decompress the downloaded ZIP file to obtain the executable of the
update program, and then execute it. |
| (4) |
|
Execute the Setup Tool for E10A-USB Emulator program to set up the
emulator software for the E10A-USB. |
- Notices
| (1) |
|
The update program downloaded in 3-(2) above cannot switch the
device group you are using to another one. |
| (2) |
|
If the update program is executed in the system where the
High-performance Embedded Workshop V.4.00.01 or earlier resides,
it will be revised to V.4.00.02. |
|
 |