|
|
 |
RENESAS TOOL NEWS on November 1, 2005: RSO-M38000T2-CPE-051101D
The Software Products Included
with the Compact Emulator M38000T2-CPE Updated |
The software products included with the compact emulator--M38000T2-CPE--for the 740 MCU family have been updated.
- The Product Including the Software Concerned
The M38000T2-CPE compact emulator is concerned.
Shipment of the M38000T2-CPE including the updated software products begins on November 1, 2005.
- Descriptions
The software products included with the M38000T2-CPE have been updated to those that can run on the High-performance Embedded Workshop V.4.00.03. They are as follows:
| (1) |
|
Emulator debugger: The 740 compact emulator debugger
This debugger has changed places with M3T-PD38M, compact emulator debugger for 740 MCU family.
For details, see RENESAS TOOL NEWS (RSO-HEW-051101D, "The 740 Compact Emulator Debugger V.1.00 Release 00 Published" published on November 1, 2005). |
| (2) |
|
C compiler package: the M3T-ICC740 evaluation version
For details, see RENESAS TOOL NEWS (RSO-M3T-ICC740-051101D: "The C Compiler Package M3T-ICC740 Revised to V.1.01 Release 01," published on November 1, 2005). |
| (3) |
|
Assembler: the M3T-SRA74 evaluation version
This assembler has changed places with M3T-SRA74M which has some restrictions (Macro commands cannot be used, etc.).
For details, see RENESAS TOOL NEWS (RSO-M3T-SRA74-051006D: "The Assembler Package M3T-SRA74 Revised to V.4.10 Release 02," published on October 7, 2005). |
Note:
Evaluation version is available, which is the same as the commercial version except that no technical support and no service to revise it are provided.
Evaluation version can be downloaded from the download site.
|
 |