|
|
 |
RENESAS TOOL NEWS on November 1, 2005: RSO-R0C38000DBW00-051101D
The 740 Compact Emulator Debugger
V.1.00 Release 00 Published |
The 740 compact emulator debugger V.1.00 Release 00 has been published.
This debugger can debug programs for the 740 family of MCUs.
- Outline
The brand-new emulator debugger can run on the High-performance Embedded
Workshop (an integrated development environment) V.4.00.03*.
- Functionality
The 740 compact emulator debugger provides the functionality equivalent
to the M3T-PD38M, another emulator debugger used for the 740 family in
combination with the compact emulator.
The 740 compact emulator debugger enables you to debug programs using the
High-performance Embedded Workshop V.4.00.03. Accordingly you are able
to accomplish seamless operations of coding, building, simulating, and
debugging under the single integrated development environment.
- Host System Requirements
| Computer | IBM PC/AT or compatible |
| OS | Windows XP, Windows 2000, Windows Me, or Windows 98SE |
- How to Get the Product
If you are using the compact emulator for the 740 family (the M38000T2-CPE),
you are able to use this brand-new emulator debugger free of charge.
This software can be downloaded from "Software download for tools".
|
 |