|
|
 |
RENESAS TOOL NEWS on November 1, 2005: RSO-M3T-ICC740-051101D
The C Compiler Package M3T-ICC740
Revised to V.1.01 Release 01 |
The C Compiler Package M3T-ICC740 has been revised from V.1.01 Release 00
to V.1.01 Release 01. This package is used for the 740 family of MCUs.
- Descriptions of Revision
| 1.1 |
|
The M3T-ICC740 has become supported by the High-performance Embedded
Workshop, so that the High-performance Embedded Workshop is installed
at the same time when the M3T-ICC740 is installed.
|
| 1.2 |
|
A simulator debugger for the 740 MCU family has been incorporated
into the High-performance Embedded Workshop. This simulator debugger
provides the functionality equivalent to the M3T-PD38SIM simulator
debugger. Because the simulator debugger enables you to debug
programs using the High-performance Embedded Workshop, you are able
to accomplish seamless operations of coding, building, simulating,
and debugging under the single integrated development environment;
that is, you need not invoke independent programs such as an editor,
compiler, simulator debugger, and emulator debugger.
For details of this simulator debugger, see its datasheets. |
NOTES:
- As a simulator debugger has been incorporated into the High-performance Embedded Workshop, the bundling of the M3T-PD38SIM,
the simulator debugger for the 740 family, will be discontinued.
- On the High-performance Embedded Workshop, the commands and
windows created by the CB38SIM (Custom Builder) do not operate.
- How to Update Your Package
Free-of-charge online update is available. So download the update
program (.exe file) from "M3T-ICC740 V.1.01 Release 00 Online Upgrade", and execute the
downloaded .exe file.
- First Ordering
When you place an order for the product, supply the following items
of information to your local Renesas Technology sales office or
distributor:
| Product Type | M3T-ICC740 |
| Version No. | V.1.01 |
| Release No. | Release 01 |
| Host OS | Windows XP, Windows Me, Windows 98, Windows 2000, or Windows NT 4.0 |
For the price of the product, contact them also.
|
 |