|
|
 |
RENESAS TOOL NEWS on November 16, 2005: RSO-HEW-051116D
A Note on Using
the High-performance Embedded Workshop (IDE) |
Please take note of the following problem in using the High-performance Embedded Workshop (IDE):
- Product Concerned
Any product of the High-performance Embedded Workshop updated using its update program
- Description
If you open the New Project Workspace dialog box, check the check box for the debugger or simulator in the New Project-7/9-Setting the Target System for Debugging section, and click the Next button when creating a workspace, no debugger option can properly be selected with the following warning message displayed:
Cannot find CPU map information
- Conditions
This problem occurs if the High-performance Embedded Workshop has been updated by performing the following procedures:
| (1) |
|
Either of the following compiler packages is installed:
- C/C++ compiler package V.7.1.03 or earlier for the SuperH RISC engine family (SHC) (Windows version)
- C/C++ compiler package V.5.0.05 or earlier for the H8, H8S, and H8SX families (H8C) (Windows version)
|
| (2) |
|
Any debugger is installed which was released in 2004 or later for the SuperH RISC engine family or the H8, H8S, and H8SX families. |
| (3) |
|
Then your High-performance Embedded Workshop is updated using its update program. |
- Workaround
Copy the folders shown below to the System\Pg\Renesas folder.
These folders reside in the System\Pg\Hitachi folder under the directory where the High-performance Embedded Workshop has been installed:
- In SHC
System\Pg\Hitachi\Sh_x_x
System\Pg\Hitachi\Hardware
- In H8C
System\Pg\Hitachi\h8_x_x
System\Pg\Hitachi\Hardware
- Schedule of Fixing the Problem
We plan to fix this problem in the next release of the product.
|
 |