|
|
 |
RENESAS TOOL NEWS on December 1, 2005: RSO-E10A-USB_1-051201D
The E10A-USB Emulator Software
Revised to V.2.02 Release 00 |
We have revised the emulator software for the E10A-USB emulators
(HS0005KCU01H and HS0005KCU02H) to V.2.02 Release 00. These emulators are
used for the SuperH RISC engine, H8S, and H8SX families of MCUs.
- Versions Concerned
Emulator software V1.0.00 through V.2.01 Release 00
for the E10A-USB emulators (HS0005KCU01H and HS0005KCU02H)
| NOTE: |
|
The above emulator software and the emulators are used for
the following MCUs of the SuperH RISC engine family:
- SH7206 group, SH7200 series (SH-2A device group)
- SH-Mobile series (New_SH-Mobile device group)
- SH7780 group, SH7780 series (SH-4A device group)
- SH7781 group, SH7780 series (SH-4A device group)
- SH7763 group, SH7760 series (SH-4A device group)
|
- Descriptions of Revision
| 2.1 |
|
Problem Fixed
The problem on using built-in trace capability, which arises when
any of the SH7206 MCU group is targeted for debugging, has been
fixed.
For details, see RENESAS TOOL NEWS RSO-E10A-USB-051116D.
("A Note on Using the E200F and E10A-USB Emulators for the SH-2A-Cored
MCUs," published on November 16, 2005).
|
| 2.2 |
|
Command Name Altered
The command name for RESETMODE, which is typed on the command line,
has been altered from RSM to RSMD. (This command is used only when
the SH-Mobile series; the SH7780 and SH7781 groups, SH7780 series;
and the SH7763 group, SH7760 series, SuperH RISC engine family of
MCUs are targeted.)
The reason is that RSM is a command name already used in Microsoft'
command script; that is, RSM is a command for managing media resources
using removable memory area.
For details of the command for RESETMODE, see the help file. |
- How to Update Your Software
Free-of-charge online update is available. The update procedures are as
follows:
| (1) |
|
Download the update program from Download site. |
| (2) |
|
Decompress the downloaded ZIP file to obtain the install program
(a setup.exe file); then execute it. |
| (3) |
|
Execute the Setup Tool for E10A-USB Emulator program to set up the
emulator software for the E10A-USB. |
- Notices
| (1) |
|
The install program obtained in 3-(2) above cannot change the
device group you are using to another one. |
| (2) |
|
If the install program is executed in the system where the
High-performance Embedded Workshop V.4.00.01 or earlier
resides, it will be updated to V.4.00.02. |
|
 |