Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS on December 16, 2005: RSO-E10A_2-051216D

A Note on Using the E10A Emulators

Please take note of the following problem in using the E10A emulators, which emulate the SuperH RISC engine family of MCUs:
  • On loading user programs to the emulator


  1. Products Concerned
    The E10A emulators, HSxxxxKCI01H and HSxxxxKCI02H
    These emulate the SuperH RISC engine family of MCUs except the SH7047F, SH7144F, and SH7145F MCUs.


  2. Description
    User programs may incorrectly be loaded into memory in the above emulators. To examine incorrect loading, conduct verification of programs in memory. If your program has incorrectly been loaded, message "verify error" will appear.


  3. Conditions
    This problem occurs if the following conditions are all satisfied:
    (1)   Any of the E10A emulators is connected with the PC via the PCI interface.
    (2)   The emulator software you are using is a High-performance Embedded Workshop edition.
    (3)   Windows 98 or Windows Me is running on the PC.


  4. Solution
    To resolve this problem, follow these steps:
    (1)   Download "E10A emulator driver for SuperH family (except for SH7047F, SH7144F and SH7145F) for Windows 98/Windows Me" from Download site.
    (2)   Update your driver to the downloaded one according to your type of emulator as follows:
    (a)   For HSxxxxKCI01H
    Overwrite your Pcidrv3.vxd file with the downloaded driver file. The Pcidrv3.vxd file is found under the C:\WINDOWS\system\drivers folder.
    (b)   For HSxxxxKCI02H
    Overwrite your Pcidrv4.vxd file with the downloaded driver file. The Pcidrv4.vxd file is found under the C:\WINDOWS\system\drivers folder.





© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal