Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS on December 16, 2005: RSO-R0C30800PMW00_2-051216D

A Note on Using
the M32C Compact Emulator Debugger
V.1.00 Release 00

Please take note of the following problem in using the M32C compact emulator debugger V.1.00 Release 00:
  • On changing the work area used by the compact emulator


  1. Product Concerned
    M32C compact emulator debugger V.1.00 Release 00


  2. Description
    You are unable to type anything in the Debug Monitor Bank Address edit box, which appears on-screen when clicking the Emulation Memory tab of the Emem dialog box.* So no changes can be made to the work area that the emulator uses.

    *   In the High-performance Embedded Workshop, if you switch a session to the one during which the debugger is used, or the Connect command is selected from the Debug menu, the Init dialog box appears. Clicking the OK button in this dialog box opens the Emem dialog box.


  3. Solution
    This problem has been resolved in the M32C compact emulator debugger V.1.00 Release 01. So download the installer of the V.1.00 Release 01 from Download site and then install it.





© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal