Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS on December 16, 2005: RSO-M30870T-EPB-051216D

A Note on Using the Compact Emulator
--M30870T2-CPE--
and the Emulation Probe for the PC7501 Emulator
--M30870T-EPB--

Please take note of the following problem in using the Compact Emulator and the Emulation Probe M30870T-EPB (used together with the PC7501 Emulator) for the M32C/87 MCU group:
  • On All the peripheral functions of the emulator MCU being halted


  1. Products Concerned
    Product Type Serial Number
    M30870T2-CPE Ending in character "A","B","C", or "D"
    M30870T-EPB Ending in character "A","B","C", or "D"

    The serial number, an 8-digit alphanumerical character, is inscribed on the label affixed to the bottom side of each product; for example, 4CM0017B.


  2. Description
    While the M30870T2-CPE or the M30870T-EPB is operating, all the peripheral functions of the emulator MCU will be halted if the following conditions are all satisfied:
    • CPU clock frequency is 24 MHz or more.
    • Eight-bit data is written into the SFR area (000000h--0003FFh) or the external area using DMAC.
    This problem arises from the malfunction of the MCU board M30870T-EPBM mounted in both of the products concerned:
    Note that the problem does not arise in actual MCUs.


  3. Solution
    We supply you with the problem-fixed M30870T-EPBM MCU board if you are encountering this problem. So substitute it for yours by going through the following steps:
    (1)   Fill in the appended free-of-charge problem-fixed MCU board application form and send it to us by E-mail or FAX. (Send one form per product concerned.)
    (2)   We will send you a problem-fixed M30870T-EPBM board. After receiving the board, substitute it for yours by following the instructions of the M30870T-EPBM User's Manual (for MCU board replacement of the M30870T2-CPE and M30870T-EPB), which is enclosed with the board; then validate the system.
    (3)   After validating the system, send back us your previous board.
    (4)   Be sure to read the M30870T-EPBM Supplementary Document, which is also enclosed with the board, before running the problem-fixed board.

    SEND TO:
    Your local Renesas Technology sales office or distributor


  4. Notes on Applying for the Board
    (1)   Application will be accepted on and after January 16, 2006.
    (2)   We will send you the problem-fixed board from February 2006 on.
    (3)   It will take 10 working days or more to ship the board after receiving your E-mail or FAX (except for the transportation period).


  5. Notes on Using the Problem-Fixed Products
    To every product concerned where the problem-fixed MCU board is mounted and the products concerned that will be shipped after this December 16 are made the following changes:

    (1)   The maximum operating clock frequency at which the SFR area of the intelligent I/O function is read out in 1 or 2 wait state is lowered from 30 to 24 MHz.
    (2)   The limitations* imposed on the compact emulator and the emulation probe concerned are modified as follows:
    • These products cannot operate at the CPU clock frequencies exceeding 24 MHz under the condition that VCC1 > VCC2.
    • If you want to operate them at the CPU clock frequencies exceeding 24 MHz, you must set bit PM13 to 1 (2 wait states) when reading the SFR area of the intelligent I/O function.

    * These limitations are read on the following:
    • Section 4.5, Notes on Using This Product, in the M30870T-EPB User's Manual
    • Section 4.2, Differences between the Actual MCU and Emulator, in the M30870T2-CPE User's Manual

    Because the above changes are those made to the specifications of the products, the following descriptions related to the products concerned are also subject to changes:
    • Notes on Using This Product in the user's manuals and release notes
    • Footnote *2 in the lists of the specifications on the Web pages
    For details, see those documents and Web pages.





© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal