Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS on December 16, 2005: RSO-HWTOOL-051216D

Hardware Tools Released
in the First Half of December 2005

We released the hardware tools listed below in the first half of December 2005.

  1. For the R8C/Tiny Series, M16C Family of 16-Bit MCUs
    (1)   The R0E521000EPB00: The emulation probe for the R8C/Tiny series
    For details, visit datasheet.
    (2)   The R0E521000CPE00: The compact emulator for the R8C/Tiny series
    For details, visit datasheet.
    (3)   The R0E521134CFG00: A converter board for connecting a 32-pin
    0.8-mm-pitch LQFP package
    (4)   The R0E521174CSJ00: A converter board for connecting a 20-pin
    0.65-mm-pitch LSSOP package
    (5)   The R0E521174CDB00: A converter board for connecting a 20-pin
    1.778-mm-pitch SDIP package
    (6)   The R0E521237CFK00: A converter board for connecting a 48-pin
    0.5-mm-pitch LQFP package
    (7)   The R0E521258CFJ00: A converter board for connecting a 52-pin
    0.65-mm-pitch LQFP package


  2. Sets of the Emulation Probe and a Converter Board for the R8C/Tiny Series
    (1)   R0E521134EPB00: A set of the R0E521000EPB00 and R0E521134CFG00
    (2)   R0E521174EPB00: A set of the R0E521000EPB00 and R0E521174CSJ00
    (3)   R0E521174EPB10: A set of the R0E521000EPB00 and R0E521174CDB00
    (4)   R0E521237EPB00: A set of the R0E521000EPB00 and R0E521237CFK00
    (5)   R0E521258EPB00: A set of the R0E521000EPB00 and R0E521258CFJ00


  3. Sets of the Compact Emulator and a Converter Board for the R8C/Tiny Series
    (1)   R0E521134CPE00: A set of the R0E521000CPE00 and R0E521134CFG00
    (2)   R0E521174CPE00: A set of the R0E521000CPE00 and R0E521174CSJ00
    (3)   R0E521174CPE10: A set of the R0E521000CPE00 and R0E521174CDB00
    (4)   R0E521237CPE00: A set of the R0E521000CPE00 and R0E521237CFK00
    (5)   R0E521258CPE00: A set of the R0E521000CPE00 and R0E521258CFJ00


  4. Ordering Information
    Product Type Type Name Comment
    R0E521000EPB00 R0E521000EPB00 None
    R0E521000CPE00 R0E521000CPE00 None
    R0E521134CFG00 R0E521134CFG00 None
    R0E521174CSJ00 R0E521174CSJ00 None
    R0E521174CDB00 R0E521174CDB00 None
    R0E521237CFK00 R0E521237CFK00 None
    R0E521258CFJ00 R0E521258CFJ00 None
    R0E521134EPB00 R0E521134EPB00 None
    R0E521174EPB00 R0E521174EPB00 None
    R0E521174EPB10 R0E521174EPB10 None
    R0E521237EPB00 R0E521237EPB00 None
    R0E521258EPB00 R0E521258EPB00 None
    R0E521134CPE00 R0E521134CPE00 None
    R0E521174CPE00 R0E521174CPE00 None
    R0E521174CPE10 R0E521174CPE10 None
    R0E521237CPE00 R0E521237CPE00 None
    R0E521258CPE00 R0E521258CPE00 None





© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal