Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS on December 26, 2005: RSO-AutoUpdate-051226D

The AutoUpdate Utility revised to V.1.00.02

We have revised the AutoUpdate Utility, an extended function of the High-performance Embedded Workshop V.4, from V.1.00.01 to V.1.00.02.

  1. Versions Concerned
    AutoUpdate Utility V.1.00.00 and V.1.00.01

    This utility is bundled with High-Performance Embedded Workshop V.4.00.00 through V.4.00.03. *

    *   To check for the version number of your High-performance Embedded Workshop, open the Help menu and select the About High-performance Embedded Workshop command.


  2. Descriptions of Revision
    2.1   Functions Introduced
    (1)   The function to show progress when downloading an updater of each product has been introduced.
    (2)   The function to choose whether to register this utility in the startup menu to start it up automatically has been added.

    2.2   Problem Fixed
    The following problem has been fixed.
    If the download of the update program of any software product is cancelled on the way in the AutoUpdate wizard, the update program may not properly update the software product when downloaded next time.
    For details, see RENESAS TOOL NEWS RSO-HEW-050601D.


  3. How to Update Your Software
    Use this AutoUpdate Utility to update your software.
    (Available on and after January 12, 2006)





© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal