|
|
 |
RENESAS TOOL NEWS on January 1, 2006: RSO-E8-060101D
The Emulator Software for the E8 Emulator
Revised to V.2.06 Release 00 |
We have revised the emulator software for the E8 on-chip debugging emulator
from V.2.04 Release 00 to V.2.06 Release 00.
- Descriptions of Revision
| 1.1 |
|
Supported MCUs Increased
Eleven members of the M16C/6N group, M16C/60 series of MCUs have been
added to the support line. They are as follows:
M306N4FC, M306N4FG, M306N5FC,
M306NKFH, M306NMFH, M306NKFJ, M306NMFJ,
M306NLFH, M306NNFH, M306NLFJ, and M306NNFJ
|
| 1.2 |
|
High-performance Embedded Workshop Updated
The High-performance Embedded Workshop included with the revised
software has been updated from V.4.00.02 to V.4.00.03.
For details of the revision of the IDE to V.4.00.03, see RENESAS
TOOL NEWS No. RSO-HEW-051001D, issued on October 1, 2005.
|
| 1.3 |
|
Emulator Debuggers Improved
The emulator software includes the following emulator debuggers:
- R8C/Tiny E8 emulator debugger V.2.02.00
- M16C/Tiny, M16C/62P E8 emulator debugger V.1.02.00
- H8 Tiny/Super Low Power E8 emulator debugger V.1.01.01
- M32C/80 E8 emulator debugger V.1.01.00
These emulator debuggers have been improved as described below.
| 1.3.1 |
|
In the R8C/Tiny E8; M16C/Tiny, M16C/62P E8; and M32C/80 E8 Emulator Debuggers
(1) User programs are downloaded into target systems much faster.
(2) Step execution is also performed at higher speed.
(3) The time-out period has been reduced.
|
| 1.3.2 |
|
In the H8 Tiny/Super Low Power E8 Emulator Debugger
The minimum value that can be typed into the System Clock dialog
box* has been changed from 2 to 1 MHz. This change is only applied
to the case where any of the following is selected as the target MCU:
H8/38076RF, H8/38086RF, H8/38327F, and H8/38347F
* After you switch to the session for using the E8 emulator in the
High-performance Embedded Workshop, select the Connect command
from the Debug menu; then the Select Emulator mode, the Power Supply,
and the System Clock dialog box open in this order.
|
|
| 1.4 |
|
Problems Fixed
The following problems have been fixed.
| 1.4.1 |
|
In All the Emulator Debuggers (in those listed in Section 1.3)
Problem: When object files written in the IEEE695 format are loaded
into the E8 or E7 emulator, and inline functions in these files are
stepped over by the emulator, the High-performance Embedded Workshop
may be shut down abnormally.
For details, see RENESAS TOOL NEWS No. RSO-E7-051116D,
issued on November 16, 2005.
|
| 1.4.2 |
|
In the R8C/Tiny E8 Emulator Debugger
Problem: When the debugger is invoked in the "Does not download
emulator firmware" mode with any member of the R8C/15 or R8C/17
series selected as the target MCU, the user program cannot
properly be loaded into the target system, and the further
operations become impossible.
|
| 1.4.3 |
|
In the H8 Tiny/Super Low Power E8 Emulator Debugger
Problem: When any member of the H8/36077F group is targeted for
debugging, a verification error arises if the value placed in
the RCCR register is changed in the Memory or Command window of
the High-performance Embedded Workshop.
|
| 1.4.4 |
|
In the M32C/80 E8 Emulator Debugger
Problem: If a value in memory is referenced or a write is made
to memory during execution of the user program, the content of
the A0 register is replaced with a wrong value.
|
|
- How to Update Your Software
Free-of-charge online update is available. If you are using the
software, download the update program from the download site, then execute it.
NOTICE*
If the update program is executed in the system where the
High-performance Embedded Workshop V.4.00.02 or earlier
resides, it will be updated to V.4.00.03.
|
 |