Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS on January 16, 2006: RSO-M3062PT3-RPD-E-060116D

A Note on Using Emulation Pods
for the M16C MCU Family
(Used Together with the PC4701 Emulator)

Please take note of the following problem in using emulation pods for the M16C family (including TS [test sample] and WS [working sample] products), which are used together with the PC4701 emulator:
  • On detecting reads from address 00000h


  1. Products Concerned
    • M3062PT3-RPD-E and M3062PT3-RPD (TS)
      for the M16C/62P and M16C/30P MCU groups

    • M3062NT3-RPD-E
      for the M16C/62N and M16C/30L MCU groups

    • M306NKT3-RPD-E and M306NKT3-RPD (WS)
      for the M16C/6N4, /6N5, /6NK, /6NL, /6NM, and /6NN MCUs; M16C/6N group

    • M306N4T3-RPD-E (spare only) and M306N4T3-RPD (WS)
      for the M16C/6N4 and /6N5 MCUs, M16C/6N group

    • M306H3T3-RPD-E and M306H3T3-RPD (WS)
      for the M306H3 MCU, M16C/6H group

    • M306H5T3-RPD-E and M306H5T3-RPD (WS)
      for the M306H5 MCU, M16C/6H group

    • M30245T3-RPD-E
      for the M30245 MCU, M16C/24 group

    • M30100T3-RPD-E
      for the M16C/10 MCU series

    NOTICE: The M306H7T3-RPD-E is not concerned (this pod is used for the M306H7 MCU, M16C/6H group, M16C/60 series, M16C family).


  2. Description
    If a read from address 00000h is detected except when an interrupt is serviced, the yellow LED lamp on the pod lights up, and to turn out it, you need to press the reset switch on the emulator.
    In some cases, however, the lamp is automatically extinguished, preventing you from being aware of abnormal reads from address 00000h.


  3. Solution
    If it is important for you to detect any read from address 00000h except when an interrupt is serviced, you had better halt the program using hardware breakpoints. To do so, enable the hardware break function and make the following settings as the event for hardware breaks:

    (1)   Event type
    DATA ACCESS
    (2)   Address settings
    Comparison Condition: (addr)==Address1, Address1: 00000h
    (3)   Data settings
    Comparison Condition: Not Specify
    Access Condition: READ


    NOTE:   The script file HB_0000H.zip(size: 159byte), where the above settings are written, is downloadable. After downloading the file, decompress and execute it from the Script window in the emulator debugger. Note, however, that you may need to modify the descriptions in the file depending on your settings of the hardware breakpoints for halting programs.


    Descriptions in the script file:
    BM HARDWARE,ON
    HB A1,00000,R
    HB OR,A1:1





© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal